HINOU.1Visitor IIForum|Forum|5 years agoFebruary 25, 2021QuestionI changed the microcontroller from STM32F733ZEI6 to STM32F723ZEI6 and it stopped working.Forum|Forum|5 years agoFebruary 25, 20212 replies787 viewsI changed the microcontroller from STM32F733ZEI6 to STM32F723ZEI6 and it stopped working.When connecting with the debugger (STM32FcubeIDE)・STM32F733ZEI6 was able to connect.・STM32F723ZEI6 was disable to connect. and The following error occurred(Details are attached).Error: failed to download Segment[1]Error: failed to download the FileWhat should I do?STM32cubeIDE-console.txtSTM32CubeProgrammerSTM32F7 series