Skip to main content
Associate
July 29, 2025
Question

Issues regarding USB DFU STM32 F7

  • July 29, 2025
  • 2 replies
  • 422 views

Hi,

 

we have issues with USB DFU where we use the PC port. I uploaded two log files: one from CubeProgrammer and one from USB log in .txt (Wireshark).

Depended the on the USB port I am using USB DFU works. From PC seems DFU is looping while using the Dock USB port everything works fine.

10:38:05:230 : Error: Uploading Option Bytes bank: 0 failed
10:38:05:245 : Error: Initializing the Option Bytes failed

 

Also, is sending abort request common used to get in dfuIDLE state, or is this something wrong.

10:14:50:757 : Time elapsed during the read operation is: 00:00:00.004
10:14:51:834 : UPLOADING ...
10:14:51:834 : Size : 1024 Bytes
10:14:51:834 : Address : 0x8000000
10:14:51:835 : Read progress:
10:14:51:835 : DFU status = 0 : OK
10:14:51:836 : DFU state = 9 : dfuUPLOAD-IDLE
10:14:51:837 : Status: 0, State: 9
10:14:51:837 : sending an abort request
10:14:51:839 : DFU status = 0 : OK
10:14:51:839 : DFU state = 2 : dfuIDLE
10:14:51:839 : setting the address pointer to address: 0x08000000
10:14:51:840 : DFU status = 0 : OK
10:14:51:840 : DFU state = 4 : dfuDNBUSY
10:14:51:840 : DFU status = 0 : OK
10:14:51:840 : DFU state = 5 : dfuDNLOAD-IDLE
10:14:51:840 : receiving packet nbr: 0
10:14:51:841 : DFU status = 0 : OK
10:14:51:841 : DFU state = 5 : dfuDNLOAD-IDLE
10:14:51:841 : sending an abort request
10:14:51:841 : DFU status = 0 : OK
10:14:51:841 : DFU state = 2 : dfuIDLE
10:14:51:841 : UpLoading data
10:14:51:845 : DFU status = 0 : OK
10:14:51:845 : DFU state = 9 : dfuUPLOAD-IDLE

 

I hope you can help me out.

2 replies

Technical Moderator
July 30, 2025

Hello @JB98 ,

Check your boot configuration, the boot pin connection and supported communication peripherals by the system bootloader following the AN4661 in section 4 Boot configuration.

Make sure to use the latest version of CubeProgrammer.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
JB98Author
Associate
July 31, 2025

Hi Imen,

Thanks for reply, but this is all set right.

We use VBUS detect to select the boot configuration as USB DFU ones USB is plugged in at start-up. So we ignore the bootpin to automate DFU.
When connecting with "Read Unprotect", it cannot (sometimes it does) upload/read its DeviceID and OptionBytes.

JB98_0-1753944599233.png

It seems something to do with unsynchronized state machines of the internal F7 bootloader and CubeProgrammer.

The system seems to be quite unstable.

 

 

JB98Author
Associate
July 31, 2025

Example with USB FS with issue device ID

JB98_1-1753945100845.png
Issue with option bytes and device ID.

JB98_2-1753945165964.png

 

Technical Moderator
August 1, 2025

Maybe you have incorrect Option Bytes data! So, verify the option bytes configuration file.

Try perform a full chip erase to disable RDP before reprogramming option bytes.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"