Light weight CubeProgrammer CLI
Can we expect to get lightweight option of the STM32CubeProgrammer for CLI applications (STM32_Programmer_CLI.exe) that does not require using STM32CubeProgrammer.
The whole STM32CubeProgrammer package is over 600MB and contains variety of unnecessary files whereas the good old STM32-ST-Link Utility is only about 35MB and can perform majority of the operation.
This is important for custom applications that internally embed ST tools to program ST32 devices. Just because I need to use UR (under reset) mode for my particular target device, I must use STM32CubeProgrammer as the STM32-ST-LINK utility does not support that. And that is quite annoying because my application now must be 600MB larger than it should be.
It would be nice to get stripped down version of the STM32CubeProgrammer.