MacOS stm32cubeprogrammer "Error: Could not find or load main class com.st.app.Main"
On a more or less clean MacOS Mojave 10.14.6, installed the Oracle JDK (jdk-12.0.2_osx-x64_bin.dmg), installed the stm32cubeprogrammer (using the workaround via commandline). Now after installation, when starting it gives an error "The application “STM32CubeProgrammer�? can’t be opened."
Opening /Applications/.../Stm32CubeProgrammers/Contents/MacOS/bin/STM32CubeProgrammer
Shows the following problem in a terminal-box:
/Applications/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammer ; exit;
Error: Could not find or load main class com.st.app.Main
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
logout
Saving session...
...copying shared history...
...saving history...truncating history files...
...completed.
[Process completed]
In another post someone was having the same problem on Linux and the advice was to install javajfx, but as mentioned, it is said the be included in the 12.0.2 JDK... Any advice on how to get it to run?