MCU STM32F733ZE doesn't START
Hello Community,
We have an issue on a design with an MCU STM32F733ZE on a custom electronic board, we don't manage to program it through STM32Cubre Programmer ("No STM32 found"). We observed that the power consumption is very low, less than 0.1mA so we assume that the MCU doesn't turn ON, we observed that the SWDIO pin is on 3.3V permanently and we couldn't drive to low level when connected to the ST-link programmer, and the level doesn't change even if we put the NRST pin to low level. On the design side, PDR pin was first floating, a resistor was not mounted, but now the resistor is mounted, the MCU behaviour doesn't change. So we wanted to know, what is the expected consumption when the MCU is powered up for the first time ? What happen if the PDR pin was floating when first power up ? The NRST pin level seems to no have any impact on the MCU, no consumption changing, no internal voltage reference change (We measure 1.1V on the internal voltage ref).
Best regards,