Skip to main content
DBonh.1
Associate III
July 30, 2025
Solved

No Octo SPI Clk with STM32N6 external loader for MX66UW1G45G

  • July 30, 2025
  • 3 replies
  • 355 views

Hi,

I have a custom board that duplicates the STM32N6 Disco schematic for an external flash MX66UW1G45G. I configured  the .ioc to configure XSPI2 and XPSIM with PN6 pin for the clk. I use STM32CubeProgrammer with the external loader activated for MX66UW1G45G. The CubeProgrammer connects via a J-Link cable, and I select the first few blocks to erase. When I click Erase Selection, the oscope shows activity on XSPIM_P2_IO0 and XSPIM_P2_IO3, but nothing on the clock. I also didn't see any activity on the NCS1, it remains high. 
The Clock Configuration tab in the .ioc file shows an active 66.66MHz clock signal to XSPI2, with HCLK as a source.

The .ioc has XSPI2 and XSPIM enabled for all three domains - FSBL, Application, and ExtMemLoader. I attached the .ioc. 

Huge thanks for help!  

Best answer by DBonh.1

The firmware turned out to be correct. The problem was incomplete installation of the chip. Most of the balls connected but a few of them didn't, including the clock. 

Thanks to @Tesla DeLorean for providing the pin defines from the driver, that was helpful. 

 

3 replies

DBonh.1
DBonh.1Author
Associate III
July 30, 2025

The repo for example external loaders doesn't seem to include N6, even though N6 loaders are included with CubeProgrammer. Is source code for the N6 loaders located somewhere else? Because the symptoms I'm seeing could be explained if the loader calling some other pin for the clock. 

https://github.com/STMicroelectronics/stm32-external-loader

Tesla DeLorean
Guru
August 1, 2025

You might find some code examples in the Keil/MDK STM32N6 Pack

The build of the Loader looks materially similar to the other STM32's, they look to use 0x34000004

MX66UW1G45G_STM32N6570-DK.stldr builds for 0x34180400, at least for v2.18.00

HAL_PWREx_EnableVddIO3

HAL_PWREx_ConfigVddIORange

PN0:AF9  XSPI_P2_DQS0

PN1:AF9  XSPI_P2_NCS1

PN2:AF9  XSPI_P2_IO0

PN3:AF9  XSPI_P2_IO1

PN4:AF9  XSPI_P2_IO2

PN5:AF9  XSPI_P2_IO3

PN6:AF9  XSPI_P2_CLK

PN8:AF9  XSPI_P2_IO4

PN9:AF9  XSPI_P2_IO5

PN10:AF9  XSPI_P2_IO6

PN11:AF9  XSPI_P2_IO7

 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
DBonh.1
DBonh.1AuthorBest answer
Associate III
August 5, 2025

The firmware turned out to be correct. The problem was incomplete installation of the chip. Most of the balls connected but a few of them didn't, including the clock. 

Thanks to @Tesla DeLorean for providing the pin defines from the driver, that was helpful.