No padding align with padding in STM32_SigningTool_CLI 2.21
So i was failing to properly flash my STM32N6 because in version STM32_SigningTool_CLI 2.21. I think it's because it doesn't align the payload. So when i flashed the board made with 2.21 it didn't recognize it and didn't load.
In version 2.20 this doesn't happen. I don't know if this is a bug or a failed configuration. But i used the same command for both of them and it worked in version 2.20.