Skip to main content
Associate
June 29, 2025
Solved

NUCLEO-N657X0-Q ST-Link eventually locks up when accessing memory when directly attached to a Mac via USB-C

  • June 29, 2025
  • 2 replies
  • 500 views

Hi,

I'm trying to work with the STM32N6. I have a NUCLEO-N657X0-Q board.

When I use an external debugger via CN1 everything is fine, however I am experiencing a lot of trouble with the ST-Link.

It seems like there is a small (0.01%) chance that attempting to access memory will cause the device to lock up.

An example of the sort of command that gets sent to the ST-Link is: `[0xf2, 0x07, 0xfc, 0xff, 0x00, 0x34, 0xcc, 0x35, 0x01]`. That is, a simple command to the ST-Link to read or write memory.

I am doing this as part of an attempt to implement support for the STM32N6 for probe-rs, however the problem seems to occur even when using ST tools. For example, the following has a good chance of locking up:

./STM32_Programmer_CLI \
 -c port=swd \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768 \
 -r32 0x34000000 32768

 Once the ST-Link has locked up, the only way to get it back is to unplug it and plug it in again. Any attempt to access the ST-Link USB endpoint will be met with silence.

In the example I've attempted to read main memory, however I see similar lockups when attempting to read ROM, or even when attempting to read register values repeatedly such as (to pick a random peripheral) 0x56028048, or even trying to read something from the ARM CoreSight block such as 0xE000ED14.

I am running ST-Link firmware V3J16M8 on the integrated debugger. This seems like it's a bug in the ST-Link, because running the link at a lower frequency reduces the failures. For example, they seem to go away entirely at around 100 kHz.

This issue only occurs when the device is attached directly to a USB-C port on the Mac. It goes away on other platforms, and it goes away when it is behind a hub.

Best answer by STOne-32

Dear @sean_od ,

The behavior observed is linked to the Errata described in this Knowledge Article FAQ : FAQ: Possible communication failure between STLINK... - STMicroelectronics Community

Let us know

STOne-32.

2 replies

sean_odAuthor
Associate
July 18, 2025

The same command appears to work when run from a Linux host. Additionally, it works from the Mac if I put a USB-C hub in between.

The problem then becomes: The ST-Link locks up when connected directly to a USB-C port on a Mac.

Are there any known issues regarding this?

STOne-32
STOne-32Best answer
Technical Moderator
December 14, 2025

Dear @sean_od ,

The behavior observed is linked to the Errata described in this Knowledge Article FAQ : FAQ: Possible communication failure between STLINK... - STMicroelectronics Community

Let us know

STOne-32.

sean_odAuthor
Associate
December 15, 2025

Thanks for the link! This does seem to be the case. I'll add a check to alert if we're trying to use a device when connected directly to the machine, and advise the user to use a hub.