Skip to main content
Associate II
August 23, 2025
Solved

NUCLEO-N657X0-Q: Unable to erase flash

  • August 23, 2025
  • 6 replies
  • 1976 views

Hi,

I've recently been trying to get an LRUN application up and running on the NUCLEO-N657X0-Q board. Similar to the posts in https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32n6570-dk-unable-to-erase-external-flash/td-p/757897, I cannot access the flash for erasure, with errors indicating to verify flash memory protection.

michaelg643_1-1755967138338.png

 

I currently have the BOOT0 jumper on 1-2 (for 0) and BOOT1 on 2-3 (for a logical 1), which should be putting me into the Development boot mode. For external loaders, I have MX25UM51245G_STM32N6570-NUCLEO selected. 

michaelg643_0-1755966866504.png

I've tried both full chip erase and sector erase, both giving me errors that tell me to verify flash memory protection.

Please advise, I'm not sure what I'm doing wrong. This is my first time attempting to flash the memory.

EDIT: I should've mentioned, I'm using STM32CubeProgrammer 2.20.0. I've tried this on both Windows 11 and Ubuntu 24.04

EDIT #2: I have also attached the verbose log file after I hit "full chip erase" and a single sector

EDIT #3: I've also tried bypassing the chip erase and loading my signed bin file into flash. That's also locked me out, as expected.

Best answer by JOT

Bumped into the same, using STM32CubeProgrammer v2.19.0 rather than v2.20 appeared to solve this.

6 replies

Associate II
August 24, 2025

Scrubbing the OTP output, I see some deltas between the output of my NUCLEO board and the "prog-locked by ST" status of table 17 of RM0486:

michaelg643_0-1756063649551.png

Per table 17 of RM0486, OTP_HW_WORD4/OTP4 should've been prog-locked by ST, and it shows as not being locked on my board.

I don't think I programmed OTP260-267, but they show as programmed. Regardless, I think those shouldn't effect the flash operation, as they seem to be intended to be used by the application only.

I've checked the voltage on the power rails of the flash chip, as well as the reset. The chip is not being held in reset (it has a 1.8V input), and the power is at a rock-solid 1.8V as well.

Associate II
August 26, 2025

Another update -

After coming home from work, I tried getting this to work again. The very first time I plugged in the NUCLEO board and tried erasing a sector, I got this:

michaelg643_0-1756167260097.png

Which is a success! however, subsequent attempts to erase the chip lead to the same issue:

michaelg643_1-1756167317723.png

 

Now, I did think to myself, "maybe there's a hardware issue", as I had success once after the board was powered off for 24 hours. I've been able to unplug the board and leave it sitting there (letting capacitors discharge) for 3 or 4 attempts so far and I have the same behavior of it successfully clearing the sector the very first time, followed by not being able to write to the flash any more. 

Unless there's something I'm missing, I don't know if I can do anything else about this.

Technical Moderator
August 26, 2025

Hello @michaelg643 ,

Make sure to perform an ST-Link upgrade from STM32CubeProgrammer.

What is the value of RDP level?

Did you try changing the position of jumper JP2 and setting the boot mode DEV_BOOT using JP2., as suggested by @RomainR. in this post : Solved: Re: NUCLEO-N657X0-Q: failed to start GDB server.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Associate II
August 26, 2025

Hi @Imen.D,

I've done the ST-Link upgrade, to version V3J16M8 STM32 Debug+VCP, with no change in behavior.

I believe there's a typo in @RomainR.'s post, as he's calling BOOT0 JP2 and BOOT1 JP1, whereas UM3417 calls them out as BOOT0 JP1 and BOOT1 JP2. regardless, I have tried all four combinations of jumper settings with BOOT0/BOOT1 and I can only connect the debugger when JP2 is set to 2-3 (JP1 is a don't care). I currently have JP1 on 1-2 and JP2 on 2-3.

michaelg643_0-1756208743963.png

 

 

I do not know how to read or set the RDP level, this is the closest menu I've found to that: 

michaelg643_1-1756209114644.png

 

Can you show me how to read it out? 

Associate II
August 27, 2025

Further research has led me to believe that RDP isn’t present on an STM32 that doesn’t have internal flash, like this one?

Technical Moderator
August 27, 2025

Ah sorry! Did you try connecting a different board for testing?

Could you please confirm if you have the same behavior when using the command line?

Try also a power cycle of the board that may resolve the issue.

Otherwise, please share the board revision details: which Nucleo-N657X0-Q (MB1940-xxx) used?

 

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
JOTBest answer
Visitor II
August 27, 2025

Bumped into the same, using STM32CubeProgrammer v2.19.0 rather than v2.20 appeared to solve this.

Associate II
August 28, 2025

I can confirm that version 2.19.0 fixes the issue!

Technical Moderator
August 28, 2025

Hi @JOT, Thank you for your help and for sharing the solution.

Thank you @michaelg643 for your confirmation.

I raised this issue internally for investigation (through Ticket number: 216448).

Sorry, for the inconvenience it may cause.

(PS: Ticket number: 216448, is only for reference and not available outside of ST).

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Technical Moderator
November 10, 2025

Hello @michaelg643 , @JOT 

This issue will be fixed in the next version of STM32CubeProgrammer V2.21.0 and will be available soon.

So, keep an eye out for the coming update.

Thank you for your understanding while we work on this for you.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Technical Moderator
November 17, 2025

Hello @michaelg643 , @JOT 

This issue is fixed in the available release STM32CubeProg V2.21.0.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"