own external loader-custom board with 1gb nor flash which is not available in bsp
Hi ST members,
Where can I find the BSP components for the NOR flash with Part No: MT28EW01GABA?which is not in h7's bsp.
If I want to create my own external loader, I need to add the MT28EW01GABA.c and MT28EW01GABA.h files to the project. However, I can't find these files anywhere. Can anyone advise on what to do?
Thank you.
Best regards,
Jr_mbd_engr

this example is given by st-employee which is for u5 with its flash ic only.