Question
Program STM32 through bus CAN
Hello,
Is it possible to program STM32* through bus CAN with STM32CubeProgrammer and STLINK-V3SET ?
If yes :
- can we program only one STM32* even if many other STM32* are connected to the bus ?
- do we need to flash a bootloader or the embedded bootloader is enough ?
Last question : can we do this directly with STM32CubeIDE ?
Thanks for reading,
Best regards,
Valentin
(*) it will be STM32H7 or STM32F7 and the code will be written with STM32CubeIDE