Setting Auto mode with STM32CubeProgrammer v2.7.0
I have just started using STM32CubeProgrammer v2.7.0 and I liked the simple and great looking UI over the other programmers. Now I would like to use Automatic mode and expect the following:
Erase the Read Out Protection (RDP) in OB or set it to "AA"
Full chip erase
Download the file
Verify
Set the Read Out Protection (RDP) in OB to "BB"
Can I do that? If yes how?
Also could you please help me understand the OB command to set the Read Out Protection (RDP) in OB to "BB"?