SetupSTM32CubeProgrammer-2.17.0.exe failed
I got this error message when trying to install the cube programmer:
This application was configured to use a bundled java runtime environment but the runtime is missing or corrrupted

I have started an jar file to see if my local jre is broken which is not the case. Is the jre taken from the jre folder besides the exe or from the system?

I am running windows 10 x64 and do have admin rights
Tried with earlier version as well. Failed also.
I have version 2.5.0 installed