STLINK V3MINIE only working in command-line mode after STM32CubeProgrammer
Without starting the STM32 Cube Programmer (GUI) I get following error message:
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.31V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
Error: ST-LINK error (DEV_UNKNOWN_MCU_TARGET)
Done
After I have started the STM32 Cube Programmer it works:
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
JTAG freq : 21333 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x93
Hard reset is performed
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 002E001C3033511835393935
ST-LINK FW : V3J15M6
Board : STLINK-V3MINIE
Voltage : 3.30V
JTAG freq : 21333 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x93
Mass erase ...
Mass erase successfully achieved
Done
The problem can be reproduced by disconnect the STLINK V3MINIE.
I am using the latest version: V2.17.0
In my boundary scan test environment I need the command line programming.
Does anyone have an idea?
Many thanks in advance
Joerg