STM32 Trusted Package Creator NO SUPPORT FOR H743
The "Introduction to secure firmware install (SFI) for STM32 MCUs" AN4992 does not list the H743 as a supported device.
The Secure Programming tab of the latest Cube Programmer V2-18-0 (Jan 20205) states it only supports STM32U0-5 & WBA.
Yet the SFI/SFIx tab isn't disabled when connected to an H743VIT6 board.
And the STM32 Trusted Package Creator allows the STM32H7 MCU to be selected as a target.
Does anyone think that's not going to be confusing to STM clients new this (mine) field?
The "STM32 Trusted Package Creator tool software description" User Manual UM2238 runs to 30+ pages of technical description, very far from user friendly.
The STM Wiki "How to deploy SSP using a step-by-step approach" only focuses on the STM32MP1 and uses hard coded values specific to that MCU.
The only video on YouTube is by Ruchit Naik a security engineer at STM who uses an AI voice.
At 3.55 into the video a chart is listed that includes STM32H7 series, but in the list the H743 is excluded!
Clearly adding encryption to the data transfer from Cube Programmer to the STM32H743 boot loader would be very easy (I could do it in a coupe of hours if I had the source code),
So why has STM MCU managers decided to blacklist the H743?