Skip to main content
Soner23
Associate
May 4, 2024
Solved

STM32Cube Programmer installation error

  • May 4, 2024
  • 12 replies
  • 9294 views

Hello,

Stm32cubeprogrammer installation does not proceed to the final stage, it remains at step 8 and is not completed. I tried the program on three different PCs with administrator rights, the result is the same, the installation does not complete.

st32prog hata.png

Best answer by Soner23

Hello @Aziz BRIGUI 

Let me share an update on the issue.
I tried to make a fresh installation with English (USA) Language Windows 11 and install the program, it was installed without any problems.
My computer's language is Turkish, I added an English language pack to this computer, then I tried the installation again and it was installed without any problems.
Turkish I cannot complete the installation with Windows 11 and Windows 10. I hope you can solve this problem as soon as possible.

12 replies

Soner23
Soner23AuthorBest answer
Associate
May 22, 2024

Hello @Aziz BRIGUI 

Let me share an update on the issue.
I tried to make a fresh installation with English (USA) Language Windows 11 and install the program, it was installed without any problems.
My computer's language is Turkish, I added an English language pack to this computer, then I tried the installation again and it was installed without any problems.
Turkish I cannot complete the installation with Windows 11 and Windows 10. I hope you can solve this problem as soon as possible.

Explorer
August 6, 2024

Thank you very much, @Soner23 . I had the same problem and thanks to you I fixed it.

Visitor II
July 5, 2025

Hello everyone, I read the topic from beginning to end, as Mr. Soner said, I was about to lose my mind with these problems...

The computer I use is win 11 pro sp3 Turkish. I added US Eng. language from the language options and installed it without any problems on the first try...