STM32CubeController doesn't recognize STM32f3348-discovery
When I open STM32CubeProgrammer (v2.21.0) it displays an error modal "Old ST-LINK firmware version. Upgrade ST-LINK firmware.
If I click the "Firmware Upgrade" button an STLinkUpgrade 3.16.8 shows up with
Current firmware: (blank)
Type: (blank)
Version: Unknown
Update to Firmware: Unknown.
The upgrade button does nothing when clicked. How do I fix this?
I downloaded the software here https://www.st.com/en/development-tools/stsw-link007.html
After running
/usr/lib/jvm/java-17-openjdk-amd64/bin/java -jar stsw-link007-v3-17-10/stsw-link007/AllPlatforms/STLinkUpgrade.jar
There is another upgrade dialog with version 3.17.10 displaying the same firmware info as above, with the upgrade button greyed out.
Other commands ive run
$ ls -l /dev/bus/usb/001/019
crw-rw----+ 1 root plugdev 189, 18 Feb 9 09:36 /dev/bus/usb/001/019
$ lsusb | grep ST
Bus 001 Device 019: ID 0483:374b STMicroelectronics ST-LINK/V2.1
$ STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.21.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== J-Link Interface =====
No J-Link/flasher probe detected.
===== STLink Interface =====
Error: Old ST-LINK firmware version. Upgrade ST-LINK firmware
-------- Connected ST-LINK Probes List --------
ST-Link Probe 0 :
ST-LINK SN : 066DFF545054897087211137
ST-LINK FW : V2J27M15
Access Port Number : 4
Board Name :
-----------------------------------------------
===== UART Interface =====
Total number of serial ports available: 33
Error: Old ST-LINK firmware version. Upgrade ST-LINK firmware
Board Name :
ST-LINK SN: 066DFF545054897087211137
Port: ttyACM0
Location: /dev/ttyACM0
Description: STM32 STLink
Manufacturer: STMicroelectronics
$ls /etc/udev/rules.d/ | grep stlink
49-stlinkv1.rules
49-stlinkv2-1.rules
49-stlinkv2.rules
49-stlinkv3.rules
99-stlink.rules
$ cat /etc/udev/rules.d/49-stlinkv2-1.rules
# stm32 nucleo boards, with onboard st/linkv2-1
# ie, STM32F0, STM32F4.
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374b", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="3752", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"