STM32CubeIDE v1.8.0 flashing error: Data mismatch found at address
Hi,
Since I updated the STM32CubeIDE to v1.8.0 each second flash process fails with Error: Data mismatch found at address. With the STM32CubeIDE v1.6.0 everything works fine.
In the project the start address of the flash area is set to 0x08010000 because on 0x08000000 the bootloader is located.
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 49FF67066584525744110987
ST-LINK FW : V2J39S7
Board : --
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x469
Revision ID : Rev X
Device name : STM32G47x/G48x
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a12924.srec
File : ST-LINK_GDB_server_a12924.srec
Size : 131168 Bytes
Address : 0x08010000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [32 96]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:03.485
Verifying ...
Error: Data mismatch found at address 0x08010000 (byte = 0xFF instead of 0x00)
Error: Download verification failed
Shutting down...
Exit.The first 8 bytes were not programmed.
MCU: STM32G474
Programmer: ST-Link/V2
On an erased flash the flash process (triggered via STM32CubeIDE Run/Debug) is working. Afterwards each second flash process fails. Maybe the problem is located in the updated STM32CubeProgrammer. I have tried different debugger settings without success.
Thanks for any help.