STM32CubeProgramer connecting to STM32H753IIK6
I'm having trouble getting the STM32CubeProgramer to connect to my STM32H753IIK6 chip using the serial port when going into boot loader mode. I'm using RESET and BOOT pins to get the chip into boot loader mode but the
STM32CubeProgramer
will not consistently connect. It seems to be very dependent on the timing of releasing RESET and BOOT to clicking connect on the programmer. Here is the error I get in the log window when it doesn't connect:14:36:29 : Serial Port COM8 is successfully opened.
14:36:30 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...This is same error I get I the chip is running and I try the connect but the chip appears to be in boot loader mode when I get this error. Repeated rebooting release of
RESET and BOOT,
clicking connect eventually results in the STM32CubeProgramer connecting and then I can erase and program the chip without any problems.
Is there anything special about the boot loader sequence and connecting to the STM32CubeProgramer that I should know about to make this more reliable?
Thanks. Pete
#stm32cubeprogramer