STM32CubeProgrammer 2.14.0 firmware update error over USB in Windows 10 64 bit
Hi,
similarly to what happened to others with previous versions of STM32CubeProgrammer, an error occurs when I proceed to download the firmware via USB connection:
Error: Write failed at address: 0x800…. (address is not always the same)
Error: failed to download Segment[0]
Error: failed to download the File
The error in log file is:
libusb control transfer error [-9] : LIBUSB_ERROR_PIPE
Even the initial connection via USB does not work correctly, as not all information is always read correctly (The initial connection fails if I use version 2.10.0 of STM32CubeProgrammer).
Similarly to what others have found, everything works correctly if the connection is made through a USB 3.0 hub. Also, everything works fine if I use DfuSeDemo software, so the problem seems to be related to the STM32 BOOTLOADER driver used by STM32CubeProgrammer.
The specs of my system are
microcontroller STM32F072RBT6
firmware version: 0x011a
device id: 0x0448
operating system: Windows 10 Pro 64 bit version 22H2
USB 3.0
Does anyone have any helpful suggestions?
Thanks!