STM32CUBEprogrammer connect fails but can program just fine in cubeIDE
Hello,
I cannot use the STM32CUBEprogrammer standalone program, however my programmer works just fine with stm32CUBEIDE V1.7. During programming in STM32cubeide the configuration is visible and it loads STM32cubeprogrammer V2.8 I copied the settings over to the standalone program since those seem to work in STM32CUBEIDE but it still does not work. I updated to the latest firmware and tried out both V2.9 and V2.8 of STM32CUBEprogrammer but neither works.
My settings: (from cubeide same settings used in cubeprogrammer)
ST-LINK SN : 6
ST-LINK FW : V2J39S7
Board : --
Voltage : 3.33V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x447
Revision ID : Rev Z
Device name : STM32L07x/L08x/L010
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0x__
I am using an ST-link compatible probe not an official one at the moment. The official one however does work. I dont mind using an official programmer but this one is a bit more convenient since it also can supply power.
https://opencircuit.nl/product/st-link-v2-stm8-stm32-programmer
Does anyone know why this problem happens? I dont think there is anything wrong with my connection. But it might be an incompatability between the official and this particular programmer, specifically with the standalone program but not the command line variant used in cubeide.