Skip to main content
SamHansen42
Associate II
October 2, 2023
Solved

STM32CubeProgrammer does not install

  • October 2, 2023
  • 2 replies
  • 2033 views

Hello, STM32cubeprogrammer fails to install, can you assist?

M1 Macbook Pro (Ventura 13.4.1)
Java Version = 1.8.0_381
STM32CubeProgrammer = 2.14.0

SamHansen42_0-1696273742002.png

 

This topic has been closed for replies.
Best answer by Sara BEN HADJ YAHYA

Hello @SamHansen42 ,

Thanks for your feedback,

Please try one of the following solutions:

1- Install CubeProgrammer using the command:

sudo xattr -cr ~/SetupSTM32CubeProgrammer-macos.app

2- In case you used the .exe installer (sudo java -jar SetupSTM32CubeProgrammer-2.14.0.exe.) and the popup occurs during the install indicating the following:

""

cp: en.stm32cubeprg-mac_v2-14-0/../../../jre: No such file or directory

Continue Installation?

""

Continue the installation and copy the downloaded jre folder manually into the CubeProg install folder. To do so, please follow the steps below:

- Copy the jre folder from the downloaded en.stm32cubeprg-mac_v2-14-0

- Open CubeProgrammer install folder

- Right click on STM32CubeProgrammer.app and select "Show Package Contents"

- Paste the jre folder

3- After the install, if CubeProgrammer couldn't be launched via GUI, please try to lanch it via CLI as follows,

- Navigate to the /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/

- type the command:

java -jar STM32CubeProgrammer

- If the jre folder exists in CubeProgrammer install folder, type the following command:

../../../jre/bin/java -jar STM32CubeProgrammer

I hope this helps!

Sara.

2 replies

ST Employee
October 16, 2023

Hello @SamHansen42 ,

Thanks for your feedback,

Please try one of the following solutions:

1- Install CubeProgrammer using the command:

sudo xattr -cr ~/SetupSTM32CubeProgrammer-macos.app

2- In case you used the .exe installer (sudo java -jar SetupSTM32CubeProgrammer-2.14.0.exe.) and the popup occurs during the install indicating the following:

""

cp: en.stm32cubeprg-mac_v2-14-0/../../../jre: No such file or directory

Continue Installation?

""

Continue the installation and copy the downloaded jre folder manually into the CubeProg install folder. To do so, please follow the steps below:

- Copy the jre folder from the downloaded en.stm32cubeprg-mac_v2-14-0

- Open CubeProgrammer install folder

- Right click on STM32CubeProgrammer.app and select "Show Package Contents"

- Paste the jre folder

3- After the install, if CubeProgrammer couldn't be launched via GUI, please try to lanch it via CLI as follows,

- Navigate to the /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/

- type the command:

java -jar STM32CubeProgrammer

- If the jre folder exists in CubeProgrammer install folder, type the following command:

../../../jre/bin/java -jar STM32CubeProgrammer

I hope this helps!

Sara.

SamHansen42
Associate II
October 23, 2023

TLDR: DO STEP 2 OF SOLUTION PROVIDED BY SARA, INSTALL THE EXE AND MANUALLY COPY THE JRE AS INDICATED

1. When entered this command I got no response from terminal.

 

2. OK, performed


2- In case you used the .exe installer (sudo java -jar SetupSTM32CubeProgrammer-2.14.0.exe.) and the popup occurs during the install indicating the following:

""

cp: en.stm32cubeprg-mac_v2-14-0/../../../jre: No such file or directory

Continue Installation?

""

Continue the installation and copy the downloaded jre folder manually into the CubeProg install folder. To do so, please follow the steps below:

- Copy the jre folder from the downloaded en.stm32cubeprg-mac_v2-14-0

- Open CubeProgrammer install folder

- Right click on STM32CubeProgrammer.app and select "Show Package Contents"

- Paste the jre folder



I would like to point out for other users, somehow I had a copy of .app directly under Applications/STMicroelectronics/. This was possibly installing using the .app instead of .exe. This caused confusion when performing step 2, i copied the jre here. Now I got rid of this. when you copy the jre I think you should copy to the .app file inside Applications/STMicroelectronics/STM32Cube.

I did this of step 3, but then realized my mistake above and corrected that. App starts


3- After the install, if CubeProgrammer couldn't be launched via GUI, please try to lanch it via CLI as follows,

- Navigate to the /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/

- type the command:

java -jar STM32CubeProgrammer

Thank you!