STM32CubeProgrammer does nothing after clicking Start Programming button
Looking for something to try. I'm want to recover from a failed firmware update of an MLite-880 from Elecevolve after their their 1-click installer. Elecevolve suggested a manual install using the firmware binary and STM32CubeProgrammer. I can put the device in its "DFU FW update mode" and connect to the device from the STM32CubeProgrammer using USB. After connect, the log shows:
08:45:07 : STM32CubeProgrammer API v2.22.0 | Windows-64Bits
08:45:35 : Disconnected from device.
08:46:01 : USB speed : Full Speed (12MBit/s)
08:46:01 : Manuf. ID : MALAHITEAM
08:46:01 : Product ID : Malahit-Lite DFU
08:46:01 : SN : 305B376E3133
08:46:01 : DFU protocol: 1.1
08:46:01 : Board : --
08:46:01 : IAP
08:46:01 : UPLOADING ...
08:46:01 : Size : 1024 Bytes
08:46:01 : Address : 0x8000000
08:46:01 : Read progress:
08:46:01 : Data read successfully
08:46:01 : Time elapsed during the read operation is: 00:00:00.053
When I click Start Programming, literally nothing happens except the progress bar at the bottom previously at 100% clears. Any information as to what these results are telling me, or suggestions as to what to try would be appreciated. I'm using V2.22.0 of STM32Cube Programmer and I have run it from both Windows 10 and 11 computers.