Skip to main content
FWege.1
Associate II
September 29, 2022
Question

STM32CubeProgrammer STM32G474 option bytes / IWDG

  • September 29, 2022
  • 3 replies
  • 1924 views

Dear all

If we clear the IWDG option (enable watchdog by hardware at bootup), we cannot undo this.

In that case we have to use the old STM32 ST-LINK Utility tool.

STM32CubeProgrammer version: v2.11.0

µC: STM32G474RBT3

The problem seems to be PC dependent!

Thanks in advance,

Franz

This topic has been closed for replies.

3 replies

Houda GHABRI
ST Employee
September 29, 2022

Hi @FWege.1​ ,

I'm not able to reproduce the issue, can you please tell me more about your PC configuration where this issue occurs?

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer-2.11.0-RC4\bin>STM32_Programmer_CLI.exe -c port=SWD -ob IWDG_SW=1

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.11.0-RC4

   -------------------------------------------------------------------

ST-LINK SN : 001900303137510839383538

ST-LINK FW : V3J9M3

Board    : STM32G474E-EVAL

Voltage   : 3.28V

SWD freq  : 24000 KHz

Connect mode: Normal

Reset mode : Software reset

Device ID  : 0x469

Revision ID : Rev B

Device name : STM32G47x/G48x

Flash size : 512 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : --

  

UPLOADING OPTION BYTES DATA ...

 Bank     : 0x00

 Address    : 0x40022020

 Size     : 20 Bytes

██████████████████████████████████████████████████ 100%

 Bank     : 0x01

 Address    : 0x40022044

 Size     : 16 Bytes

██████████████████████████████████████████████████ 100%

 Bank     : 0x02

 Address    : 0x40022070

 Size     : 8 Bytes

██████████████████████████████████████████████████ 100%

OPTION BYTE PROGRAMMING VERIFICATION:

Option Bytes successfully programmed

Time elapsed during option Bytes configuration: 00:00:01.173

Houda

Piranha
Principal III
September 29, 2022

Connect mode: Under Reset

Reset mode : Hardware reset

FWege.1
FWege.1Author
Associate II
October 4, 2022

Hello together

First thanks for your answers.

The problem occurs sporadically - mostly on the Windows 7 systems.

 Betriebssystemname   Microsoft Windows 7 Professional

Version 6.1.7601 Service Pack 1 Build 7601

Systemtyp         x64-basierter PC

Maybe it has something to do with the watchdog – I’m not sure. How is the watchdog handled during programming/flashing?

The only difference in the logfiles is following line – which occurs on my windows 10 system, if everything works as expected

 16:27:13:483 : WriteOB function terminated with connection error due to OB_Launch

Thanks Piranha – but unfortunately that doesn't help