Skip to main content
Associate II
December 3, 2025
Solved

STM32CubeProgrammer v2.21 breaks External Loader

  • December 3, 2025
  • 1 reply
  • 138 views

Hello,

Our project is based on the STM32WBA65MI, and we have an external flash chip on the board that we use STM32CubeProgrammer w/a custom external loader to program. This worked well with STM32CubeProgrammer v2.20, but when I updated to STM32CubeProgrammer v2.21, suddenly I was unable to connect to the board using the external loader.

This happens as soon as I select the external loader and

JFisherLegato_0-1764769774872.png

If I select verbosity level 3, this is what I see:

08:50:10:520 : Selected loader: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/ExternalLoader/MX25R6435_STM32WBA65-LEGATO.stldr
08:50:10:520 : Error: Flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/ExternalLoader/MX25R6435_STM32WBA65-LEGATO.stldr cannot be loaded.

Here's the StorageInfo:

struct StorageInfo __attribute__((section(".Dev_Info"))) const StorageInfo = {
 "MX25R6435F_Legato", // Device Name + version number
 SPI_FLASH, // Device Type
 0x00000000, // Device Start Address
 0x800000, // Device Size in Bytes
 0x1000, // Programming Page Size
 0xFF, // Initial Content of Erased Memory

 // Specify Size and Address of Sectors (view example below)
 {
 { 0x800, // Sector Numbers,
 0x1000 }, // Sector Size

 { 0x00000000, 0x00000000 }
 }
};

I'm running Windows 11 Pro 25H2 if that makes a difference. The flash part we're writing to is the MX25R6435F.

My linker script is as follows:

/* Entry Point */
ENTRY(Init)

/* Generate 2 segment for Loader code and device info */
PHDRS {Loader PT_LOAD ; SgInfo PT_LOAD ; }

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1); /* end of "RAM" Ram type memory */

_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */

/* Memories definition */
MEMORY
{
 RAM_D1 (xrw) : ORIGIN = 0x20000004, LENGTH = 512K-4
}

/* Sections */
SECTIONS
{

 .isr_vector :
 {
 	. = . + 0x1FC; /* ISR vector offset */
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >RAM_D1 :Loader

 .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >RAM_D1

 .ARM : {
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 } >RAM_D1 :Loader

 .preinit_array :
 {
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 } >RAM_D1 :Loader

 .init_array :
 {
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 } >RAM_D1 :Loader

 .fini_array :
 {
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 } >RAM_D1 :Loader

 /* Used by the startup to initialize data */
 _sidata = LOADADDR(.data);

 /* Initialized data sections into "RAM" Ram type memory */
 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */

 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */

 } >RAM_D1 :Loader

 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss section */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)

 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM_D1 :Loader
 
 /* The program code and other data into RAM type memory */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)

 KEEP (*(.init))
 KEEP (*(.fini))
	KEEP (*Loader_Src.o ( .text* ))
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >RAM_D1 : Loader
 
 .Dev_Info :
 {
 	__Dev_Info_START = .;
 	*(.Dev_Info*)
 	KEEP(*(.Dev_Info))
 	__Dev_Info_END = .;
 } >RAM_D1 :SgInfo
 
 /* Constant data into "FLASH" Rom type memory */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >RAM_D1 :Loader
 
 /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM_D1 :Loader

 /* Remove information from the compiler libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }

 .ARM.attributes 0 : { *(.ARM.attributes) }
}

For what it's worth, I also set up the Init() function to simply return 0, but CubeProgrammer still threw the same error.

Thank you,

Jonathan

Best answer by Aziz BRIGUI

Hi @JFisher-Legato,

Issue is fixed in the latest STM32CubeProgrammer release available here.

Aziz

1 reply

Aziz BRIGUI
Technical Moderator
December 10, 2025

Hello @JFisher-Legato,

Seems there's an issue when parsing external loaders starting @0x00000000 in STM32CubeProgrammer v2.21.0. I have logged an internal tracker for this to get further insights (Internal ticket number: 223560).

 

In the meantime, could you try changing the Device Start Address in StorageInfo to an address space you're not using for other memories (E.g: 0x70000000).

Aziz

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Aziz BRIGUI
Aziz BRIGUIBest answer
Technical Moderator
February 25, 2026

Hi @JFisher-Legato,

Issue is fixed in the latest STM32CubeProgrammer release available here.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.