Skip to main content
SDiMo.1
Associate
March 31, 2022
Question

STM32CubeProgrammer won't erase target device flash.

  • March 31, 2022
  • 2 replies
  • 2603 views

Hi all. I am using STM32CubeProgrammer with an STM32G474VET6 target system on a Windows 10 box with a USB-connected STLink module. The programmer is v2.10.0, and the STL firmware is v2J3757.

My problem is that the Cube programmer doesn't seem to be able to perform a mass erase on the target prior to programming. When I try to program, I get the following message:

Error: failed to erase memory

The Full chip erase button fails as well with

Error: Mass erase operation failed.Please verify flash protection

Flash write protection is not enabled on the target. I can erase and program just fine with the STM32 ST-LINK Utility. Also, Cube programs successfully if the target device flash is blank.

I'm happy to provide any of the target settings on request.

Any ideas?

Thanks,

Mike

This topic has been closed for replies.

2 replies

SDiMo.1
SDiMo.1Author
Associate
March 31, 2022

More info - I set the output verbosity level to 3 (highest) and harvested the following:

11:43:44:651 : MASS ERASE ...

 11:43:44:652 : Flash erase...

 11:43:44:655 : halt ap 0

 11:43:44:655 : w ap 0 reg 15 PC  (0x20000000) 

 11:43:44:657 : w ap 0 reg 17 MSP (0x20000500) 

 11:43:44:657 : w ap 0 reg 16 xPSR (0x01000000) 

 11:43:44:667 : w ap 0 @0x20000C80 0x00000200 bytes Data 0x00000000

 11:43:44:668 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00

 11:43:44:681 : w ap 0 @0x20000004 0x00000848 bytes Data 0xB672B580

 11:43:44:681 : Init flashloader...

 11:43:44:681 : halt ap 0

 11:43:44:681 : w ap 0 reg 0 R0  0x00000001

 11:43:44:681 : w ap 0 reg 1 R1  0x00000000

 11:43:44:681 : w ap 0 reg 2 R2  0x00000000

 11:43:44:682 : w ap 0 reg 3 R3  0x00000000

 11:43:44:682 : w ap 0 reg 4 R4  0x00000000

 11:43:44:682 : w ap 0 reg 5 R5  0x00000000

 11:43:44:683 : w ap 0 reg 6 R6  0x00000000

 11:43:44:683 : w ap 0 reg 7 R7  0x00000000

 11:43:44:683 : w ap 0 reg 8 R8  0x00000000

 11:43:44:683 : w ap 0 reg 9 R9  0x00000000

 11:43:44:686 : w ap 0 reg 10 R10 0x00000000

 11:43:44:688 : w ap 0 reg 11 R11 0x00000000

 11:43:44:688 : w ap 0 reg 12 R12 0x00000000

 11:43:44:689 : w ap 0 reg 13 SP  0x00000000

 11:43:44:690 : w ap 0 reg 14 LR  0x20000001

 11:43:44:690 : w ap 0 reg 15 PC  0x20000005

 11:43:44:690 : w ap 0 reg 16 xPSR 0x01000000

 11:43:44:691 : w ap 0 reg 17 MSP 0x20000C48

 11:43:44:691 : w ap 0 reg 18 PSP 0x00000000

 11:43:44:691 : run ap 0

 11:43:45:648 : halt ap 0

 11:43:45:648 : r ap 0 reg 0 R0  0x00000001

 11:43:45:648 : Loader mass erase...

 11:43:45:648 : Error: Mass erase operation failed.Please verify flash protection

Technical Moderator
April 6, 2022

Hello @SDiMo.1​ ,

Did you try to connect under reset?

Imen

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"