Question
STM32CubeProgrammer - write to memory without reset
Hi,
I want to write U32 value to EEPROM (STM32L07) without resetting after writing is done.
1) This writes the value, but then resets the MCU: STM32_Programmer_CLI.exe -c port=SWD mode=normal freq=8000 -w32 0x8080000 0x3 -v
2) I tried this: STM32_Programmer_CLI.exe -c port=SWD mode=hotplug freq=8000 -w32 0x8080000 0x3 - but it returns: Error: Failed to download data! If it's a Flash memory, it may be not erased or protected
Any idea how to write the values? Maybe I would use something like:
halt MCU -> write to memory (eeprom) -> run MCU / or reset MCU
Thank you.