STM32CubeProgrammer ZULU8 Jre recommended
STM32CubeProgrammer requires a Java™ Runtime Environment (JRE) to execute and In April 2019, Oracle decided to change their economic model around Java.
Since this date the Oracle JVM beyond version 1.8u211 becomes non-free for professional usage
For STM32CubeProgrammer tool, STMicroelectronics recommend to use the Zulu 8 JRE and this how you can install it
Note:
Development team is working on bundling the JRE with STM32CubeProgrammer 2.6.0 installer", there will be no more need to install a JRE to use STM32CubeProgrammer
Instructions to install and launch STM32CubeProgrammer (V2.5.0) with ZULU 8
To avoid issues linked to java (javafx missing library), some workarounds are available using the ZULU 8 which is basically an openjdk with and integrated javafx
Windows(32/64 bits):
1) Download Zulu Jre 8 from (https://cdn.azul.com/zulu/bin/zulu8.44.0.13-ca-fx-jre8.0.242-win_x64.zip)
2)Unzip the package in your machine
3) Change the Zulu\bin\java.exe settings to fit the high resolution screens settings:
-Right click on Zulu\bin\java .exe
-Select properties, then the compatibility tab --> Settings and tick override high DPI scaling behavior [System]
4)Install STM32CubeProgrammer with ZULU JRE8:
-Run CMD with administrator privilege.
-Install STM32CubeProgrammer "Zulu"\bin\java.exe -jar SetupSTM32CubeProgrammer-2.5.0.exe
5) After installation, you can launch the tool now through CMD
-Open CMD window(no admin rights are needed)
- Go to STM32CubeProgrammer install location: "....\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
-Launch with this command: "Zulu_install_location\bin\java.exe -jar STM32CubeProgrammer.exe"
Linux(64 bits):
1) Download Zulu jre 8 from (https://cdn.azul.com/zulu/bin/zulu8.44.0.13-ca-fx-jre8.0.242-linux_x64.tar.gz)
2) Unzip the package in your machine.
3)Install STM32CubeProgrammer with Zulu jre 8:
-open a new terminal and run the following:
"home/usr/Desktop/zulu8.44.0.13-ca-fx-jre8.0.242-linux_x64/bin/java -jar STM32CubeProgrammer-2.5.0.exe"
4) Go to STMCubeProgrammer install path /bin
5) Run "Vi STM32CubeProgrammer" and modify the java keyword by the path of the unzipped zulu package .
example(.../zulu8.44.0.13-ca-fx-jre8.0.242-linux_x64/bin/java -jar $DIR/STMCubeProgrammerLauncher)
6) Run command ":./STM32CubeProgrammer"
Macos:
1) Download the zulu jre 8 from(https://cdn.azul.com/zulu/bin/zulu8.44.0.13-ca-fx-jre8.0.242-macosx_x64.zip)
2) Unzip the package in your machine.
3) Install STM32CubeProgrammer with Zulu jre 8:
-Open terminal :chmod +x /Users/usr/Downloads/zulu8.44.0.13-ca-fx-jre8.0.242-macosx_x64/bin/java
-Run Terminal (if it does not work run it in admin mode (with sudo -i))
.../zulu8.44.0.13-ca-fx-jre8.0.242-macosx_x64/bin/java -jar .../STM32CubeProgrammer-2.5.0.exe
4) Run STMCubeProgrammer
-Go to STM32CubeProgrammer install location
"cd Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/Macos/bin"
-.../zulu8.44.0.13-ca-fx-jre8.0.242-macosx_x64/bin/java -jar ./STM32CubeProgrammer
Note:In some cases on console could be displayed this exception related to openjdk distribution (like liberica and zulu):
java.lang.ClassNotFoundException: com.sun.deploy.uitoolkit.impl.fx.HostServicesFactory :
this exception could be safely ignored and it doesn’t affect the STM32CubeProgrammer
To avoid this exception you can replace java.exe by javaw.exe while launching the GUI