STM32F030C8T6> connect with STLINKv2 & STCube Programmer..... I want to flash firmware using SWO port. Pin connections are TVCC(pin1), SWCLK(9), SWIO(7), STM32rst(15) GND(12).
Error: No STM32 target found! This is the CONSTANT message I get from the STCUBE software. I can see reference voltage from my board but actually connecting to the chip is impossible Error: No STM32 target found!, Error: No STM32 target found!, Error: No STM32 target found!
I don't understand what the problem is; I just want a single access event via SWO pins so I can woosh the firmware onboard. My developer uses some kind of el cheapo Chinese clone so can't advise me as to why using the official ARM kit is proving to be such a pain. Accessing PDI pins on an ATMEL chip is something I can do in seconds using ICE/Studio.... what's the secret to the ARM equivalent?
Thanks