STM32F769I-DISCO, MB1225 B-02, A201800875
Hi,
I have another problem with the board "STM32F769I-DISCO, MB1225 B-02, A201800875".
I wanted to restore the original firmware of the board.
Download from ST site the image "10_2020\32F769IDISCOVERY_demo\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex". Loaded it according to the "32F769IDISCOVERY_demo\readme.txt" file. I used two applications for loading:
1)STM32 ST-LINK Utility 4.6
2)STM32CubeProgrammer 2.4.0
with the same result, load the main picture with ST logo and stops. Nothing else. I think the reason is the wrong firmware revision. Before deleting the original " FW" I checked System Info and their FirmWare revision is 1.2, but I didn't find anywhere on ST site firmware such revision.
But when I do the same on the previous board
" Board: STM32F769I-DISCO, MB1225 B-02, A192400285
Screen : MB1166 A-02, A192400688"
with the
"10_2020\32F769IDISCOVERY_demo\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex". Loaded it according to the "32F769IDISCOVERY_demo\readme.txt" file. with STM32CubeProgrammer 2.4.0 all is working as expected.
So many problems with the board with the latest revision, with which we worked a lot normally in the past.
And the main problem is that the touchscreen does not work in our program (the separate case was opened).
Please help us to resolve it.
Best regards,
Dmitry