STM32G4,Set Chip Read Protect,then can not connect the Chip。(had solved)
I used STM32CubeProgrammer,And Set Chip Read Protection(RDP:0xCC),
Now The Chip can not be connect By JLINK STLINK either Usart�?
is there some method to reset the protection level?
the problem had be solved,detail below:
Level 2: No debug
In this level, the protection level 1 is guaranteed. In addition, the Cortex®-M4 debug port, the
boot from RAM (boot RAM mode) and the boot from System memory (boot loader mode)
are no more available. In user execution mode (boot FLASH mode), all operations are
allowed on the Flash Main memory. On the contrary, only read operations can be performed
on the option bytes.