Associate III
July 16, 2021
Solved
STM32H745 Core M4 boot0 address update in option byte issue.
- July 16, 2021
- 3 replies
- 2054 views
I have tested changing boot0 addresses for both the cores (M7 & M4) by STM32CubeProgrammer in ST-LINK mode. It is working properly.
When I tried to implement same logic in SPI boot mode, M4_boot0 address is not updating. Where as M7_boot0 address is able to update.
I tried connecting STM controller in UART mode with STM32CubeProgrammer, there also M7_boot0 address is able to update but while updating M4_boot0 address STM32CubeProgremmer gives error in updating M4_boot0 address.
Please refer attachment for STM32CubeProgrammer logs in UART mode.
Why option bytes are updating only in ST-LINK mode, what is wrong in SPI and UART mode ?
Please suggest the changes if needed.
Thank you.
Vaibhav.