STM32H747I-DISCO and STM32CubeProgrammer 2.5.0
Hi All,
I have STM32H747I-DISCO board with a built-in STLink-V3E. I am trying to falsh the MCU, but no matter what I do, I cannot get STM32CubeProgrammer 2.5.0 to recognise the board.
I plug the board into Win10 PC via a micro-USB cable in the ST-Link-V3E socket (CN2). The board powers up and displayes demo software that came with it. JP6 jumper is set to STlk.
I fire up STM32CubeProgrammer 2.5.0 which says "No ST-link detected".
I have installed STLink009 drivers, however, I also don't see the board under the "USB Composite divce" list in the Device manager.
Is the board faulty or am I doing something wrong?
Thank you!