Associate
October 21, 2023
Question
STM32H747I-DISCO Flash Example
- October 21, 2023
- 3 replies
- 1778 views
"DCMI_SnapshotMode DCMI Snapshot Mode example"
I am a beginner and would appreciate help with the following Readme.txt:
"In order to make the program work, you must do the following :
- Open your preferred toolchain
- For each target configuration (STM32H747I_DISCO_CM7 and STM32H747I_DISCO_CM4) :
- Rebuild all files
- Load images into target memory
- After loading the two images, you have to reset the board in order to boot (Cortex-M7) and CPU2 (Cortex-M4) at once.
- Run the example"
I hope the attached photo indicates that I have completed "Load images into target memory".
How do I complete the remaining steps?