STM32TrustedPackageCreator_CLI still needs a DISPLAY to be defined
I want to run STM32TrustedPackageCreator_CLI in docker. Unfortunately it requires a display, and is throwing an error without it:
qt.qpa.xcb: could not connect to display
qt.qpa.plugin: From 6.5.0, xcb-cursor0 or libxcb-cursor0 is needed to load the Qt xcb platform plugin.
qt.qpa.plugin: Could not load the Qt platform plugin "xcb" in "" even though it was found.
This application failed to start because no Qt platform plugin could be initialized. Reinstalling the application may fix this problem.
Available platform plugins are: vnc, minimalegl, linuxfb, wayland, wayland-egl, eglfs, xcb, vkkhrdisplay, offscreen, minimal.
Aborted (core dumped)
Is there a way to run it headless? CLI implies running without graphics?