Skip to main content
paolog
Associate III
September 17, 2024
Question

STM32TrustedPackageCreator HSM_P11_Lib.dll error

  • September 17, 2024
  • 2 replies
  • 860 views

I'm trying to program an HSM Smart Card but I'm facing with this error: "HSM_P11_Lib.dll not found"

I'm running the updated version (2.17) of STM32TrustedPackageCreator 32-bit on a Windows 10 PC (32-bit as well). The device manager shows me that the driver for the smart card reader is correclty working, as well as the HSM Smart Card. The STM32TrustedPackageCreator works fine with the same reader and same card on another Windows 10 PC, but in 64-bit.

The DLL library is in the bin folder (which is in the system path), and properties show me it's the 32 bit version.

Where could be the problem?

2 replies

Aziz BRIGUI
Technical Moderator
October 9, 2024

Hello @paolog

Thanks for bringing this to our attention. Issue is already tracked internally. Internal Ticket number : 192569.

For now, the workaround is to use 64-bit OS. 

PS : The 32-bit version of STM32CubeProgrammer works as expected for Windows 10 64-bit (The DLL is successfully loaded).

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
paolog
paologAuthor
Associate III
October 12, 2024

Thank you @Aziz BRIGUI