STM32U585 communication error DEV_TARGET_CMD_ERROR
Hi All,
Greetings
We are using STM32U585 on custom board with Trust zone enabled and now facing a connection issue with stm cube programmer in hotplug mode, now unable to connect to the microcontroller and getting ST-LINK error as : DEV_TARGET_CMD_ERROR.
When NRST is low continuously(pressing the Reset Switch) the connection to the controller through Cube Programmer is happening, but we are unable to change any option bytes, to revert back to Non Trust Zone Code. Once the reset switch(NRST) is high, it is going back to the same error.
Any suggestions for this issue and how can we resolve this?
Thanks and Regards
Philip