Skip to main content
Associate III
September 16, 2024
Question

stm32WB. How to reset to factory settings?

  • September 16, 2024
  • 1 reply
  • 1181 views

Hello,  I have a problem with the return of the STM32WB to the factory settings 

When I use the next command 

STM32_Programmer_CLI.exe -c port=SWD -w32 0x5800040C 0x00008000

that looks like that 

08bf8040-d86f-4e8c-8268-a610e0253820 (1).jpeg

But finally, when I read FUSE I saw that Stake was not removed and FUSE (was not updated, because I uploaded an old version for testing). 

FUS.jpg

I used the custom PCB board and didn't use BOOT0 during my command if it was necessary.

So does any alternative exist to return factory settings?

 

My problem started from the moment when I did not correctly upload Stack and BLE didn't start working, details are here

https://community.st.com/t5/stm32-mcus-wireless/stm32wb-capricious-fuss-how-to-erase-chip-to-factory-settings/td-p/715780

1 reply

RonilAuthor
Associate III
September 17, 2024

I have the setting for my BLE

 

bin>STM32_Programmer_CLI -c port=SWD -ob displ
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.17.0
 -------------------------------------------------------------------

ST-LINK SN : 6798040132124647524B4E00
ST-LINK FW : V2J37S7
Board : --
Voltage : 3.15V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled


UPLOADING OPTION BYTES DATA ...

 Bank : 0x00
 Address : 0x58004020
 Size : 96 Bytes

██████████████████████████████████████████████████ 100%

 Bank : 0x01
 Address : 0x58004080
 Size : 8 Bytes

██████████████████████████████████████████████████ 100%


OPTION BYTES BANK: 0

 Read Out Protection:

 RDP : 0xAA (Level 0, no protection)

 BOR Level:

 BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)

 User Configuration:

 nBOOT0 : 0x1 (nBOOT0=1 Boot from main Flash)
 nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise system Flash)
 nSWBOOT0 : 0x0 (BOOT0 taken from the option bit nBOOT0)
 SRAM2RST : 0x1 (SRAM2 is not erased when a system reset occurs)
 SRAM2PE : 0x1 (SRAM2 parity check disable)
 nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
 nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
 nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
 WWDGSW : 0x1 (Software window watchdog)
 IWDGSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
 IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
 IWDGSW : 0x1 (Software independent watchdog)
 IPCCDBA : 0x0 (0x0)

 Security Configuration Option bytes - 1:

 ESE : 0x1 (Security enabled)

 PCROP Protection:

 PCROP1A_STRT : 0x1FF (0x80FF800)
 PCROP1A_END : 0x0 (0x8000800)
 PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
 PCROP1B_STRT : 0x1FF (0x80FF800)
 PCROP1B_END : 0x0 (0x8000800)

 Write Protection:

 WRP1A_STRT : 0xFF (0x80FF000)
 WRP1A_END : 0x0 (0x8000000)
 WRP1B_STRT : 0xFF (0x80FF000)
 WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1

 Security Configuration Option bytes - 2:

 SFSA : 0xCE (0x80CE000)
 FSD : 0x0 (System and Flash secure)
 DDS : 0x1 (CPU2 debug access disabled)
 C2OPT : 0x1 (SBRV will address Flash)
 NBRSD : 0x0 (SRAM2b is secure)
 SNBRSA : 0xF (0x2003BC00)
 BRSD : 0x0 (SRAM2a is secure)
 SBRSA : 0xA (0x20032800)
 SBRV : 0x33800 (0x20000000)