Skip to main content
FRieb.1
Associate II
November 24, 2021
Question

STMCubeProgrammer - Start after programming not possible with Readout Protection Level 1

  • November 24, 2021
  • 2 replies
  • 743 views

I want to start the application after programming it and setting the readout protection. But when the readout protection is set to level 1 this is no longer possible. With level 0 it works as usual.

This topic has been closed for replies.

2 replies

TDK
Super User
November 24, 2021

How specifically are you starting the application with STM32CubeProgrammer and what error message or undesired behavior do you get when it is "no longer possible"?

"If you feel a post has answered your question, please click ""Accept as Solution""."
FRieb.1
FRieb.1Author
Associate II
November 25, 2021

When I select <Run after programming> the application runs after programming if the readout protection is at level 0.

If the readout protection is at level 1 the application is not running after programming. The Log says " Application is running, Please Hold on..." and "Start operation achieved successfully" but it doesn`t work.0693W00000GYo1QQAT.png