STSPIN32G4 not detected after first programming – Boot0 not exposed
Hello,
I’m working with the STSPIN32G4. I was able to program the MCU once successfully, but since then neither STM32CubeIDE nor STM32CubeProgrammer are able to detect it anymore.
The main issue is that I did not expose the BOOT0 pin on my board, so I can’t easily force it into system bootloader mode.
Has anyone faced a similar issue?
Is there any workaround without physical access to the BOOT0 pin?
Would SWD still work if the application firmware misconfigured the debug pins?
Any suggestions for recovering the MCU in this situation?
I’d really appreciate any help or guidance.
Thanks in advance!