Skip to main content
Associate II
February 20, 2025
Question

The only routine folder in the \bin\ExternalLoader folder in the cubemxprogrammer2.18.0 installation folder is the stldr file

  • February 20, 2025
  • 1 reply
  • 446 views

我使用 H750VBTx 芯片读取寄存器0x1FF1E7FE返回值如下所示

keanlee0721_0-1740065135381.png


参考 https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-2-18-0-released/td-p/747840 文章,我的芯片的 bootloader 版本是否无法使用 stm32cubeprogramme2.18.0 对外部 qspi 闪存进行编程?
我在哪里可以获得 \bin\ExternalLoader 文件夹中的最新可用例程?

哪个版本的 CubeProgrammer 有这个例子?

非常感谢


愿你安好

 

1 reply

Aziz BRIGUI
Technical Moderator
February 21, 2025

Hello @keanlee0721

I don't quite understand your request. Do you want to program external memory via the bootloader interface ?

If yes, this is not possible for most STM32 system bootloaders (For now only possible for STM32H7R/S using the OBL external loader).

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.