Skip to main content
Visitor II
January 12, 2026
Question

UART Bootloader for STM32F412VGTx

  • January 12, 2026
  • 3 replies
  • 254 views

As mentioned in the AN2606 document for STM32F412VGTx MCU(Custom chip), I am using USART2 (PD6/PD5) for UART bootloader using STM32CubeProgrammer. But I am getting an error message as attached. Help me to resolve this issue.

Screenshot 2026-01-09 124126.png

3 replies

Andrew Neil
Super User
January 12, 2026

Welcome to the forum.

 


@shanmukhi wrote:

STM32F412VGTx MCU (Custom chip)


STM32F412VGTx is not a custom chip.

Did you mean STM32F412VGTx on a custom board ?

If so, you need to give details of that board:

How to write your question to maximize your chances to find a solution

 


@shanmukhi wrote:

Screenshot 2026-01-09 124126.png


So have you checked those things?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
January 12, 2026

@Andrew Neil wrote:

Did you mean STM32F412VGTx on a custom board ?


If so, is it a known-good commercial product, or your own design?

Have you checked the design against Application note AN4488, "Getting started with STM32F4xxxx MCU hardware development" ?

Has this board ever worked ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User
January 12, 2026

One of these is likely wrong:

  • Ensure power rails are all connected correctly. All pins.
  • Ensure VCAP voltage is 1.2 V
  • Hold BOOT0 high during reset to boot into the bootloader.
  • Ensure wiring is correct.
"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
January 12, 2026

Any signals on PA10 or PB11 that might be recognized as initial contact?

You only get one-shot at reset to make a connection, if that fails you must with BOOT=HIGH to try again.

Present schematic for what you've implemented, saves everyone have to guess at causes..

 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..