unable to programme STM32L452 in DFU mode through STM32CubeProg version 2.4.0
Hi!
I tried to use STM32CubeProg version 2.4.0 with Nucleo-L452RE by using repository example : stm32cube_fw_l4_v1150\STM32Cube_FW_L4_V1.15.0\Projects\NUCLEO-L452RE\Applications\USB_Device\DFU_Standalone
As shown in the screenshot, the board is able to enumerate itself and after selecting USB interface out of many like UART/STLINK/ OTA it shows USB1 port with serial no. 206XXX, but when trying to load DFU file, its window does not show/ recognise DFU whereas the same is present in the destination folder.
- Kindly advice where I misunderstood the whole process?
- Whether Cube Programmer have been tested with any STM32 platform through USB DFU?