Unable to update firmware on Nucleo-144 with STM32H743ZIT
I have 2 Nucleo-144 with STM32H743ZIT. I've been using one to do development, but something I did seems to have corrupted something.
My OS is windows 7 professional.
When I plug the USB in the virtual com port does not appear. However, I know the driver is installed because the VCP does appear when I plug in the one I've never used. This tells me two things, the USB cable is working and the driver is installed.
I connected the "bad" board and tried to update it's firmware with STM32CubeProgrammer, but the ST-LINK doesn't show up in the list. The "good" board will connect when I click the Connect button and when disconnect, if I start the update firmware process, ST-LINK shows up in the list as it should.
A few days ago, I was working with a USB memory stick and wanted to eject it, but I ejected STM32-STlink and it seems thereafter, I can't get the "bad" board to connect. It had been working flawlessly until I did that.
When I plug in the "good" board, the STM32-STlink device shows up. When I plug in the "bad" board, no device appears in the list of devices to eject.
What can I do to restore the functionality of the "bad" board? I've reinstalled everything from STM32CubeProgrammer to the USB driver to the ST-LINK program using the install files from STMicroelectronics website.