Updating STM32F373 over USB DFU Fails to Connect
I'm able to connect to my STM32F373 board over a USB virtual port com successfully. I'm also able to set BOOT0 high via a jumper and boot into the bootloader. The Linux 'dmesg' command shows:
[3552008.377434] usb 3-2: new full-speed USB device number 101 using xhci_hcd
[3552008.526223] usb 3-2: New USB device found, idVendor=0483, idProduct=df11, bcdDevice=22.00
[3552008.526227] usb 3-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[3552008.526229] usb 3-2: Product: STM32 BOOTLOADER
[3552008.526230] usb 3-2: Manufacturer: STMicroelectronics
[3552008.526231] usb 3-2: SerialNumber: 2077345D2039
However when I run the STM32CubeProgrammer, it does not connect to the STM32F373 or even show it listed in the USB Port dropdown box. It shows 'No DFU detected'.
I have set the boot jumper on my board and it does seem to be detected as 'STM32 BOOTLOADER' via the 'lsusb' command.
Am I able to use the USB DEVICE in CubeMX as a virtual port com, and then also use it as a USB DFU mode when it's in boot mode?
Any ideas on what I could try?
Best,