USB DFU Firmware update while RDP1
Hello Team,
Refering to this Thread :
We want to achieve same ,
Can I upgrade the firmware using USB DFU, with RDP set to level 1?
We are fine setting RDP1 -> RDP0 and Erase Flash, then Flash the Firmware.
I tried with Cubeprogrammers and CLI , but unroftunately USB1 ( STM32 Bootloader in PC device manager ) not showing and connection does not happen. Tried making BOOT0 pin high when Reset.
However , Actual plan is jump to system bootloader from User code through jump address.
Regards,