Skip to main content
taz1000
Associate II
February 24, 2019
Question

USER_APP Flash start address=0x08006000, but STLINK erases the internal flash from 0x08004000

  • February 24, 2019
  • 0 replies
  • 610 views

I'm using STM32F401RB, which has an internal 128KB flash.

IAP bootloader is using about 20KB. So, I set USER_APP's flash address to 0x08006000 (24KB)

When I download the USER_APP hex file with STLINK UTIL or STM32CubeProgrammer, they erase the flash from 0x08004000 (16KB).

So, it erases a part of IAP bootloader.

What should I do to fix this ?

Additional Info :

When I change USER_APP's flash address to 0x08008000 (32KB), the download tools erase from 0x08008000 (32KB).

Then, IAP bootloader and USER APP work fine.

Thanks...

---------------------------------------------------------------------------------------------

Self-answer

In RM0368, I found that STM32F401RB's 128KB eflash is divided into

  • 4 sectors of 16KB
  • 1 sector of 64KB

Since the eflash erasing will have a boundary as the sector sizes,

the erasing from 24KB is not possible.0690X000006DoESQA0.png

* I had worked with other MCU which has 1KB page or something else.

So, I'm get confused.

This topic has been closed for replies.