Posted on May 16, 2013 at 16:031. Is there an example project available for the SPC564A? 2. More specifically, is there a SPC5 Studio BSP for the eval board that ST and Freescale jointly sell?3. Is there any support for the eTPU2 in SPC5 Studio and/or is any support planned?I am impressed by the SPC5 Studio software, but because of the unusual way it creates projects (the component concept) it will be very difficult to use without an example. I know that it is possible to create a new component, but without at least a minimal example you would be effectively porting the entire environment to a new architecture.