Code gets stuck after enableInterrupts() and it does not function as per the logic. #include "stm8l15x.h"#include "stm8l15x_gpio.h"#include "stm8l15x_exti.h"#include "stm8l15x_rtc.h"#include "stm8l15x_itc.h"#include "stm8l15x_clk.h"#define WAKEUP_GPIO_PORT GPIOE#define WAKEUP_GPIO_PORT GPIOE#define ICC_WAKEUP_GPIO_PIN GPIO_Pin_6static void RTC_Config(void){ /* Configures the RTC */ CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1); CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE); RTC_WakeUpClockConfig(RTC_WakeUpClock_CK_SPRE_16bits); RTC_ITConfig(RTC_IT_WUT, ENABLE); /* Enable Interrupts*/ }void Delay(__IO uint32_t nCount){ for (; nCount != 0; nCount--);}void main(void){ GPIO_Init(GPIOC, GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init( WAKEUP_GPIO_PORT, ICC_WAKEUP_GPIO_PIN, GPIO_Mode_In_FL_IT); /* Enable Rising edge port PE6 for wake up conter */ EXTI->CR2 = 0x10; /* RTC configuration -------------------