Skip to main content
Associate
May 15, 2024
Solved

Login issue - STM32CubeIDE and STM32MX

  • May 15, 2024
  • 11 replies
  • 8016 views

I downloaded version 1.15.1 of the STM32 IDE, but when I start a new project and select the STM32F103C8T6 as the MCU, the first image appears. However, when I try to update the firmware, it asks for a login, and the second image appears. I have searched in several places and realized that this is an error that can occur since versions 1.12/1.13. I have tried changing the network connections to active provider (native, manual, and direct), but it doesn't work. (I'm not sure how the manual one works, but I also saw that it's not good to keep using manual mode). Does anyone have any suggestions? The same problem occurs in STM32MX, and I have also tried changing the internet connection.

inouee_0-1715807624184.png (First image)

inouee_1-1715807726813.png(second image)

 

    Best answer by mƎALLEm

    Dear all,

    This is an issue some CubeMx/CubeIDE users are facing since yesterday and the issue was escalated internally to be fixed asap. Dedicated teams are working on it.

    11 replies

    Visitor II
    December 27, 2024

    This problem still remains for 1.17.0 cubeIDE for Mac and Windows.